LTE TDD
For Waveform Playback (ARB) capability.
Configure PRACH carrier aggrecation (CA). This button is shown when a PRACH carrier is selected in the categories of the upper pane.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<n>:PRACh:CONFig:CAGGregation <string> |
|
SCPI Example |
:RAD:LTET:WAV:CCAR:PRAC:CONF:CAGG "CAConfig:CC20M" :RAD:LTET:WAV:CCAR:PRAC:CONF:CAGG? |
|
Notes |
Set only (Immediate Action) <string>: "name:value,name:value,…" |
|
State Saved |
No |
|
Preset |
1 Carrier – 10 MHz Refer to the element definition of the data part below. |
|
Range |
Component Carriers (pulldown menu) 1 Carrier - 10 MHz 1 Carrier - 15 MHz 1 Carrier - 20 MHz 2 Carriers - 10 MHz + 10 MHz 2 Carriers - 10 MHz + 20 MHz 2 Carriers - 20 MHz + 20 MHz Refer to the element definition of the data part below. |
|
Initial S/W Revision |
A.14.00 |
Element definition of the data part. The preset value is basically the same as the default value of each setting definition.
|
Settings |
Symbols in the data part |
Values in the data part |
Preset values |
|---|---|---|---|
|
CA Carrier Config |
CAConfig |
CC10M|CC15M|CC20M|CC10MCC10M|CC10MCC20M|CC20MCC20M |
CC10M |
Sets the carrier configuration type of carrier aggregation.
|
SCPI Command |
N/A |
|
Notes |
No SCPI, GUI only, Read and Write |
|
State Saved |
No |
|
Preset |
1 Carrier: 10 MHz |
|
Range |
1 Carrier: 10 MHz | 1 Carrier: 15 MHz | 1 Carrier: 20 MHz | 2 Carriers: 10 MHz + 10 MHz | 2 Carriers: 10 MHz + 20 MHz | 2 Carriers: 20 MHz + 20 MHz |
|
Initial S/W Revision |
A.14.00 |